Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static RollingLineBuilder.Types |
RollingLineBuilder.Types.GEODESIC
Create a single geodesic line on the surface.
|
static RollingLineBuilder.Types |
RollingLineBuilder.Types.MANUAL
Creates a single line on the surface where the maximum force is to be applied.
|
static RollingLineBuilder.Types |
RollingLineBuilder.Types.PRESSURE
Create multiple lines on the surface where the tangential for each line is constant on intersecting plane sections.
|
static RollingLineBuilder.Types |
RollingLineBuilder.Types.STEPPED_PRESSURE
Create a saw tooth set of curves on the surface where the tangential for each line is constant on intersecting plane sections.
|
Modifier and Type | Method and Description |
---|---|
RollingLineBuilder.Types |
RollingLineBuilder.type()
Returns the value identifying what type of manufacturing process is to be applied to the surface for bending.
|
static RollingLineBuilder.Types |
RollingLineBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RollingLineBuilder.Types |
RollingLineBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RollingLineBuilder.Types[] |
RollingLineBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RollingLineBuilder.setType(RollingLineBuilder.Types type)
License requirements: nx_ship_concept ("Ship Concept") OR nx_ship_mfg_prep ("Ship Manufacturing") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.