Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static RollingLineBuilder.ConstructionMethodTypes |
RollingLineBuilder.ConstructionMethodTypes.ASYMPTOTE
Use an initial value method and march along and create the asymptotic lines.
|
static RollingLineBuilder.ConstructionMethodTypes |
RollingLineBuilder.ConstructionMethodTypes.HIGHLIGHT
Use an initial value method and march along the highlight (zero degree isocline) at each subsequent location.
|
static RollingLineBuilder.ConstructionMethodTypes |
RollingLineBuilder.ConstructionMethodTypes.MARCHING_ANGLE
Use an initial value method and march along the varying normals at each subsequent location.
|
static RollingLineBuilder.ConstructionMethodTypes |
RollingLineBuilder.ConstructionMethodTypes.MARCHING_CURVATURE
Use an initial value method and march along the varying normals at each subsequent location adjusting the final direction by the sheet curvature.
|
static RollingLineBuilder.ConstructionMethodTypes |
RollingLineBuilder.ConstructionMethodTypes.MAXIMUM_CURVATURE
Use an initial value method and march along the maximum curvature at each subsequent location.
|
static RollingLineBuilder.ConstructionMethodTypes |
RollingLineBuilder.ConstructionMethodTypes.MINIMUM_CURVATURE
Use an initial value method and march along the minimum curvature at each subsequent location.
|
static RollingLineBuilder.ConstructionMethodTypes |
RollingLineBuilder.ConstructionMethodTypes.PARALLEL_PLANE
Use a parallel plane approach to develop the pressure line.
|
Modifier and Type | Method and Description |
---|---|
RollingLineBuilder.ConstructionMethodTypes |
RollingLineBuilder.constructionMethodOption()
Returns the value specifying which construction method to use for creating the rolling line.
|
static RollingLineBuilder.ConstructionMethodTypes |
RollingLineBuilder.ConstructionMethodTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RollingLineBuilder.ConstructionMethodTypes |
RollingLineBuilder.ConstructionMethodTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RollingLineBuilder.ConstructionMethodTypes[] |
RollingLineBuilder.ConstructionMethodTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RollingLineBuilder.setConstructionMethodOption(RollingLineBuilder.ConstructionMethodTypes constructionMethodOption)
License requirements: nx_ship_concept ("Ship Concept") OR nx_ship_mfg_prep ("Ship Manufacturing") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.