Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static PlateStockBuilder.ThicknessSourceOptions |
PlateStockBuilder.ThicknessSourceOptions.FILE
The thickness is defined by a table of standard thicknesses for different material and material grades in CSV file.
|
static PlateStockBuilder.ThicknessSourceOptions |
PlateStockBuilder.ThicknessSourceOptions.LIST
The thickness is defined by a list of standard thicknesses for different material and material grades.
|
Modifier and Type | Method and Description |
---|---|
PlateStockBuilder.ThicknessSourceOptions |
PlateStockBuilder.thicknessSourceOption()
Returns the thickness source option.
|
static PlateStockBuilder.ThicknessSourceOptions |
PlateStockBuilder.ThicknessSourceOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlateStockBuilder.ThicknessSourceOptions |
PlateStockBuilder.ThicknessSourceOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlateStockBuilder.ThicknessSourceOptions[] |
PlateStockBuilder.ThicknessSourceOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PlateStockBuilder.setThicknessSourceOption(PlateStockBuilder.ThicknessSourceOptions thicknessSourceOption)
License requirements: nx_ship_detail ("Ship Detail Design") OR nx_ship_basic ("Ship Basic Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.