Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static PlateBuilder.TightnessOptions |
PlateBuilder.TightnessOptions.AIR_TIGHT |
static PlateBuilder.TightnessOptions |
PlateBuilder.TightnessOptions.NON_TIGHT |
static PlateBuilder.TightnessOptions |
PlateBuilder.TightnessOptions.OIL_TIGHT |
static PlateBuilder.TightnessOptions |
PlateBuilder.TightnessOptions.WATER_TIGHT |
Modifier and Type | Method and Description |
---|---|
PlateBuilder.TightnessOptions |
PlateBuilder.tightness()
Returns the tightness, which defines the plate is tight (air tight, oil tight, water tight) or non tight.
|
static PlateBuilder.TightnessOptions |
PlateBuilder.TightnessOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlateBuilder.TightnessOptions |
PlateBuilder.TightnessOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlateBuilder.TightnessOptions[] |
PlateBuilder.TightnessOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PlateBuilder.setTightness(PlateBuilder.TightnessOptions tightness)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.