Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static PenetrationRequest.RequestType |
PenetrationRequest.RequestType.MULTIPLE |
static PenetrationRequest.RequestType |
PenetrationRequest.RequestType.SINGLE |
Modifier and Type | Method and Description |
---|---|
PenetrationRequest.RequestType |
PenetrationRequestBuilder.requestType()
Returns the request type
License requirements: None. |
static PenetrationRequest.RequestType |
PenetrationRequest.RequestType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PenetrationRequest.RequestType |
PenetrationRequest.RequestType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PenetrationRequest.RequestType[] |
PenetrationRequest.RequestType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PenetrationRequestBuilder.setRequestType(PenetrationRequest.RequestType enumRequestType)
License requirements: nx_penetration_mgmt ("Penetration Management") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.