Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static OrientationAngleMethodsBuilder.MethodTypes |
OrientationAngleMethodsBuilder.MethodTypes.ALIGNED
Angle is the same as the previous or following region.
|
static OrientationAngleMethodsBuilder.MethodTypes |
OrientationAngleMethodsBuilder.MethodTypes.ANGLE
Angle is defined by specifying a constant angle from a reference object.
|
static OrientationAngleMethodsBuilder.MethodTypes |
OrientationAngleMethodsBuilder.MethodTypes.VECTOR
Angle is defined by specifying a vector to align with.
|
Modifier and Type | Method and Description |
---|---|
OrientationAngleMethodsBuilder.MethodTypes |
OrientationAngleMethodsBuilder.angleMethod()
Returns the method used to calculate the angle.
|
static OrientationAngleMethodsBuilder.MethodTypes |
OrientationAngleMethodsBuilder.MethodTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientationAngleMethodsBuilder.MethodTypes |
OrientationAngleMethodsBuilder.MethodTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientationAngleMethodsBuilder.MethodTypes[] |
OrientationAngleMethodsBuilder.MethodTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OrientationAngleMethodsBuilder.setAngleMethod(OrientationAngleMethodsBuilder.MethodTypes angleMethod)
License requirements: nx_ship_basic ("Ship Basic Design") OR nx_ship_detail ("Ship Detail Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.