Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Method and Description |
---|---|
ItFrameListItemBuilder |
ItFramesBuilder.createInterTransverseFrameListItem()
Create a list containing all required info to generate inter transverse frame.
|
ItFrameListItemBuilder |
ItFrameListItemBuilderList.findItem(int index)
Returns the object at the input index.
|
ItFrameListItemBuilder[] |
ItFrameListItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ItFrameListItemBuilderList.append(ItFrameListItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
ItFrameListItemBuilderList.append(ItFrameListItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ItFrameListItemBuilderList.erase(ItFrameListItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
ItFrameListItemBuilderList.erase(ItFrameListItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ItFrameListItemBuilderList.findIndex(ItFrameListItemBuilder obj)
Finds the index where the input object appears.
|
void |
ItFrameListItemBuilderList.insert(int location,
ItFrameListItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
ItFrameListItemBuilderList.setContents(ItFrameListItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
ItFrameListItemBuilderList.swap(ItFrameListItemBuilder object1,
ItFrameListItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.