Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static EdgeReinforcementBuilder.OrientationMethods |
EdgeReinforcementBuilder.OrientationMethods.FACE_NORMAL |
static EdgeReinforcementBuilder.OrientationMethods |
EdgeReinforcementBuilder.OrientationMethods.VECTOR |
Modifier and Type | Method and Description |
---|---|
EdgeReinforcementBuilder.OrientationMethods |
EdgeReinforcementBuilder.orientationMethod()
Returns the method used to orient the edge reinforcement.
|
static EdgeReinforcementBuilder.OrientationMethods |
EdgeReinforcementBuilder.OrientationMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeReinforcementBuilder.OrientationMethods |
EdgeReinforcementBuilder.OrientationMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeReinforcementBuilder.OrientationMethods[] |
EdgeReinforcementBuilder.OrientationMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EdgeReinforcementBuilder.setOrientationMethod(EdgeReinforcementBuilder.OrientationMethods orientationMethod)
License requirements: nx_ship_basic ("Ship Basic Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.