Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static EdgeReinforcementBuilder.EndCutTypes |
EdgeReinforcementBuilder.EndCutTypes.CONNECTED |
static EdgeReinforcementBuilder.EndCutTypes |
EdgeReinforcementBuilder.EndCutTypes.FLANGE_FREE |
static EdgeReinforcementBuilder.EndCutTypes |
EdgeReinforcementBuilder.EndCutTypes.SNIPED |
Modifier and Type | Method and Description |
---|---|
EdgeReinforcementBuilder.EndCutTypes |
EdgeReinforcementBuilder.endCutEnd()
Returns the end cut to use at the end of the edge reinforcement system.
|
EdgeReinforcementBuilder.EndCutTypes |
EdgeReinforcementBuilder.endCutStart()
Returns the end cut to use at the start of the edge reinforcement system.
|
static EdgeReinforcementBuilder.EndCutTypes |
EdgeReinforcementBuilder.EndCutTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeReinforcementBuilder.EndCutTypes |
EdgeReinforcementBuilder.EndCutTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeReinforcementBuilder.EndCutTypes[] |
EdgeReinforcementBuilder.EndCutTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EdgeReinforcementBuilder.setEndCutEnd(EdgeReinforcementBuilder.EndCutTypes endCutEnd)
License requirements: nx_ship_basic ("Ship Basic Design") . |
void |
EdgeReinforcementBuilder.setEndCutStart(EdgeReinforcementBuilder.EndCutTypes endCutStart)
License requirements: nx_ship_basic ("Ship Basic Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.