Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static EdgeCutBuilder.VersionID |
EdgeCutBuilder.VersionID.NX85
This feature builder is used to edit an existing NX85 - NX9 edge cut feature.
|
static EdgeCutBuilder.VersionID |
EdgeCutBuilder.VersionID.NX901
This feature builder is used to create or edit an NX901 or beyond feature.
|
Modifier and Type | Method and Description |
---|---|
static EdgeCutBuilder.VersionID |
EdgeCutBuilder.VersionID.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeCutBuilder.VersionID |
EdgeCutBuilder.VersionID.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeCutBuilder.VersionID[] |
EdgeCutBuilder.VersionID.values()
Returns an array that contains the values for this enum.
|
EdgeCutBuilder.VersionID |
EdgeCutBuilder.version()
Returns the version of the feature (used to determine which properties and methods are applicable) during edit.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.