Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Method and Description |
---|---|
DeckListItemBuilder |
DecksBuilder.createDeckListItemBuilder()
Creates a
DeckListItemBuilder . |
DeckListItemBuilder |
DeckListItemBuilderList.findItem(int index)
Returns the object at the input index.
|
DeckListItemBuilder[] |
DeckListItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
DeckListItemBuilderList.append(DeckListItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
DeckListItemBuilderList.append(DeckListItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
DeckListItemBuilderList.erase(DeckListItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
DeckListItemBuilderList.erase(DeckListItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
DeckListItemBuilderList.findIndex(DeckListItemBuilder obj)
Finds the index where the input object appears.
|
void |
DeckListItemBuilderList.insert(int location,
DeckListItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
DeckListItemBuilderList.setContents(DeckListItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
DeckListItemBuilderList.swap(DeckListItemBuilder object1,
DeckListItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.