public static class FlangeBuilder.OffsetTypeOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_INSIDE
The flange is offset to the inside of the face
|
static int |
_OUTSIDE
The flange is offset to the outside of the face
|
static FlangeBuilder.OffsetTypeOptions |
INSIDE
The flange is offset to the inside of the face
|
static FlangeBuilder.OffsetTypeOptions |
OUTSIDE
The flange is offset to the outside of the face
|
Modifier and Type | Method and Description |
---|---|
static FlangeBuilder.OffsetTypeOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlangeBuilder.OffsetTypeOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlangeBuilder.OffsetTypeOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final FlangeBuilder.OffsetTypeOptions INSIDE
public static final FlangeBuilder.OffsetTypeOptions OUTSIDE
public static final int _INSIDE
public static final int _OUTSIDE
public static FlangeBuilder.OffsetTypeOptions valueOf(int value)
public static FlangeBuilder.OffsetTypeOptions valueOf(String name)
public static FlangeBuilder.OffsetTypeOptions[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.