public static class ContourFlangeBuilder.SweepTypeOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CHAIN |
static int |
_FINITE |
static int |
_SYMMETRIC |
static int |
_TO_END |
static ContourFlangeBuilder.SweepTypeOptions |
CHAIN |
static ContourFlangeBuilder.SweepTypeOptions |
FINITE |
static ContourFlangeBuilder.SweepTypeOptions |
SYMMETRIC |
static ContourFlangeBuilder.SweepTypeOptions |
TO_END |
Modifier and Type | Method and Description |
---|---|
static ContourFlangeBuilder.SweepTypeOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ContourFlangeBuilder.SweepTypeOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ContourFlangeBuilder.SweepTypeOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final ContourFlangeBuilder.SweepTypeOptions FINITE
public static final ContourFlangeBuilder.SweepTypeOptions SYMMETRIC
public static final ContourFlangeBuilder.SweepTypeOptions TO_END
public static final ContourFlangeBuilder.SweepTypeOptions CHAIN
public static final int _FINITE
public static final int _SYMMETRIC
public static final int _TO_END
public static final int _CHAIN
public static ContourFlangeBuilder.SweepTypeOptions valueOf(int value)
public static ContourFlangeBuilder.SweepTypeOptions valueOf(String name)
public static ContourFlangeBuilder.SweepTypeOptions[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.