Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Method and Description |
---|---|
VariableRadiusPointsBuilder |
VariableRadiusPointsBuilderList.findItem(int index)
Returns the object at the input index.
|
VariableRadiusPointsBuilder[] |
VariableRadiusPointsBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
VariableRadiusPointsBuilder |
FlowBlendBuilder.newControlPoint()
The control point object's create function
License requirements: solid_modeling ("SOLIDS MODELING") . |
Modifier and Type | Method and Description |
---|---|
void |
VariableRadiusPointsBuilderList.append(VariableRadiusPointsBuilder object)
Appends an object to the list
License requirements: None. |
void |
VariableRadiusPointsBuilderList.append(VariableRadiusPointsBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
VariableRadiusPointsBuilderList.erase(VariableRadiusPointsBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
VariableRadiusPointsBuilderList.erase(VariableRadiusPointsBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
VariableRadiusPointsBuilderList.findIndex(VariableRadiusPointsBuilder obj)
Finds the index where the input object appears.
|
void |
VariableRadiusPointsBuilderList.insert(int location,
VariableRadiusPointsBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
VariableRadiusPointsBuilderList.setContents(VariableRadiusPointsBuilder[] objects)
Sets the contents of the entire list.
|
void |
VariableRadiusPointsBuilderList.swap(VariableRadiusPointsBuilder object1,
VariableRadiusPointsBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.