Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static UnsewBuilder.UnsewTool |
UnsewBuilder.UnsewTool.EDGE
selected edges to split faces
|
static UnsewBuilder.UnsewTool |
UnsewBuilder.UnsewTool.FACE
selected faces to unsew
|
Modifier and Type | Method and Description |
---|---|
UnsewBuilder.UnsewTool |
UnsewBuilder.toolOption()
Returns the tool option
License requirements: None. |
static UnsewBuilder.UnsewTool |
UnsewBuilder.UnsewTool.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static UnsewBuilder.UnsewTool |
UnsewBuilder.UnsewTool.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static UnsewBuilder.UnsewTool[] |
UnsewBuilder.UnsewTool.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
UnsewBuilder.setToolOption(UnsewBuilder.UnsewTool toolOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.