Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static UnsewBuilder.UnsewOutput |
UnsewBuilder.UnsewOutput.ONE_BODY_FOR_CONNECTED_FACES
One body for connected unsewn faces
|
static UnsewBuilder.UnsewOutput |
UnsewBuilder.UnsewOutput.ONE_BODY_FOR_EACH_FACE
One body for every unsewn face.
|
Modifier and Type | Method and Description |
---|---|
UnsewBuilder.UnsewOutput |
UnsewBuilder.output()
Returns the output body option
License requirements: None. |
static UnsewBuilder.UnsewOutput |
UnsewBuilder.UnsewOutput.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static UnsewBuilder.UnsewOutput |
UnsewBuilder.UnsewOutput.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static UnsewBuilder.UnsewOutput[] |
UnsewBuilder.UnsewOutput.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
UnsewBuilder.setOutput(UnsewBuilder.UnsewOutput output)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.