Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static TubeBuilder.Output |
TubeBuilder.Output.MULTIPLE_SEGMENTS
multiple segments output
|
static TubeBuilder.Output |
TubeBuilder.Output.SINGLE_SEGMENT
single segment output
|
Modifier and Type | Method and Description |
---|---|
TubeBuilder.Output |
TubeBuilder.outputOption()
Returns the output topology option
License requirements: None. |
static TubeBuilder.Output |
TubeBuilder.Output.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TubeBuilder.Output |
TubeBuilder.Output.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TubeBuilder.Output[] |
TubeBuilder.Output.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TubeBuilder.setOutputOption(TubeBuilder.Output outputOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.