Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static TrimCurveBuilder.SecondBoundingObjectOptions |
TrimCurveBuilder.SecondBoundingObjectOptions.SELECT_OBJECT
Select object
|
static TrimCurveBuilder.SecondBoundingObjectOptions |
TrimCurveBuilder.SecondBoundingObjectOptions.SPECIFY_PLANE
Define plane
|
Modifier and Type | Method and Description |
---|---|
TrimCurveBuilder.SecondBoundingObjectOptions |
TrimCurveBuilder.secondBoundingObjectOption()
Returns the second bounding object option
License requirements: None. |
static TrimCurveBuilder.SecondBoundingObjectOptions |
TrimCurveBuilder.SecondBoundingObjectOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimCurveBuilder.SecondBoundingObjectOptions |
TrimCurveBuilder.SecondBoundingObjectOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimCurveBuilder.SecondBoundingObjectOptions[] |
TrimCurveBuilder.SecondBoundingObjectOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimCurveBuilder.setSecondBoundingObjectOption(TrimCurveBuilder.SecondBoundingObjectOptions secondboundingObjectOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.