Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static TrimCurveBuilder.InteresectionMethods |
TrimCurveBuilder.InteresectionMethods.INFERRED
Inferred
|
static TrimCurveBuilder.InteresectionMethods |
TrimCurveBuilder.InteresectionMethods.USER_DEFINED
User defined
|
Modifier and Type | Method and Description |
---|---|
TrimCurveBuilder.InteresectionMethods |
TrimCurveBuilder.interesectionMethod()
Returns the method to be used to determine the intersections
License requirements: None. |
static TrimCurveBuilder.InteresectionMethods |
TrimCurveBuilder.InteresectionMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimCurveBuilder.InteresectionMethods |
TrimCurveBuilder.InteresectionMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimCurveBuilder.InteresectionMethods[] |
TrimCurveBuilder.InteresectionMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimCurveBuilder.setInteresectionMethod(TrimCurveBuilder.InteresectionMethods interesectionMethod)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.