Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static TrimCurveBuilder.FirstBoundingObjectOptions |
TrimCurveBuilder.FirstBoundingObjectOptions.SELECT_OBJECT
Select object
|
static TrimCurveBuilder.FirstBoundingObjectOptions |
TrimCurveBuilder.FirstBoundingObjectOptions.SPECIFY_PLANE
Define plane
|
Modifier and Type | Method and Description |
---|---|
TrimCurveBuilder.FirstBoundingObjectOptions |
TrimCurveBuilder.firstBoundingObjectOption()
Returns the first bounding object option
License requirements: None. |
static TrimCurveBuilder.FirstBoundingObjectOptions |
TrimCurveBuilder.FirstBoundingObjectOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimCurveBuilder.FirstBoundingObjectOptions |
TrimCurveBuilder.FirstBoundingObjectOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimCurveBuilder.FirstBoundingObjectOptions[] |
TrimCurveBuilder.FirstBoundingObjectOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimCurveBuilder.setFirstBoundingObjectOption(TrimCurveBuilder.FirstBoundingObjectOptions firstBoundingObjectOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.