Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static TrimBodyBuilder.DirectionType |
TrimBodyBuilder.DirectionType.INVALID |
static TrimBodyBuilder.DirectionType |
TrimBodyBuilder.DirectionType.NEGATIVE_NORMAL |
static TrimBodyBuilder.DirectionType |
TrimBodyBuilder.DirectionType.POSITIVE_NORMAL |
Modifier and Type | Method and Description |
---|---|
TrimBodyBuilder.DirectionType |
TrimBodyBuilder.trimDirection()
Returns the trim direction of the trim body feature
License requirements: None. |
static TrimBodyBuilder.DirectionType |
TrimBodyBuilder.DirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimBodyBuilder.DirectionType |
TrimBodyBuilder.DirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimBodyBuilder.DirectionType[] |
TrimBodyBuilder.DirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimBodyBuilder.setTrimDirection(TrimBodyBuilder.DirectionType direction)
Sets the trim direction of the trim body feature
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.