Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static TrimAndExtendBuilder.OperationType |
TrimAndExtendBuilder.OperationType.MAKE_CORNER |
static TrimAndExtendBuilder.OperationType |
TrimAndExtendBuilder.OperationType.UNTIL_SELECTED |
Modifier and Type | Method and Description |
---|---|
TrimAndExtendBuilder.OperationType |
TrimAndExtendBuilder.operation()
Returns the trim extend type
License requirements: None. |
static TrimAndExtendBuilder.OperationType |
TrimAndExtendBuilder.OperationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimAndExtendBuilder.OperationType |
TrimAndExtendBuilder.OperationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimAndExtendBuilder.OperationType[] |
TrimAndExtendBuilder.OperationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimAndExtendBuilder.setOperation(TrimAndExtendBuilder.OperationType operation)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.