Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ToolingBoxBuilder.RefCsysType |
ToolingBoxBuilder.RefCsysType.ABSOLUTEIN_DISPLAYED_PART
reference ABS in displayed part
|
static ToolingBoxBuilder.RefCsysType |
ToolingBoxBuilder.RefCsysType.SELECTED_CSYS
reference the selected csys
|
static ToolingBoxBuilder.RefCsysType |
ToolingBoxBuilder.RefCsysType.WCS
reference WCS
|
Modifier and Type | Method and Description |
---|---|
ToolingBoxBuilder.RefCsysType |
ToolingBoxBuilder.referenceCsysType()
Returns the reference csys type
License requirements: None. |
static ToolingBoxBuilder.RefCsysType |
ToolingBoxBuilder.RefCsysType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ToolingBoxBuilder.RefCsysType |
ToolingBoxBuilder.RefCsysType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ToolingBoxBuilder.RefCsysType[] |
ToolingBoxBuilder.RefCsysType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ToolingBoxBuilder.setReferenceCsysType(ToolingBoxBuilder.RefCsysType referenceType)
License requirements: ug_mold_design ("UG MOLD") OR nx_electrode_wizard ("NX Electrode Wizard") OR prog_die_wizard ("UG/Progressive Die Wizard") OR studio_free_form ("STUDIO FREE FORM") OR features_modeling ("FEATURES MODELING") OR solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.