Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ThroughCurvesBuilder.BodyPreferenceTypes |
ThroughCurvesBuilder.BodyPreferenceTypes.SHEET
Sheet
|
static ThroughCurvesBuilder.BodyPreferenceTypes |
ThroughCurvesBuilder.BodyPreferenceTypes.SOLID
Solid
|
Modifier and Type | Method and Description |
---|---|
ThroughCurvesBuilder.BodyPreferenceTypes |
ThroughCurvesBuilder.bodyPreference()
Returns the body type options
License requirements: None. |
static ThroughCurvesBuilder.BodyPreferenceTypes |
ThroughCurvesBuilder.BodyPreferenceTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ThroughCurvesBuilder.BodyPreferenceTypes |
ThroughCurvesBuilder.BodyPreferenceTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ThroughCurvesBuilder.BodyPreferenceTypes[] |
ThroughCurvesBuilder.BodyPreferenceTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ThroughCurvesBuilder.setBodyPreference(ThroughCurvesBuilder.BodyPreferenceTypes bodyPreference)
License requirements: features_modeling ("FEATURES MODELING") OR nx_freeform_1 ("basic freeform modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.