Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ThroughCurveMeshBuilder.EmphasisType |
ThroughCurveMeshBuilder.EmphasisType.BOTH
Emphasis on both primary and cross strings.
|
static ThroughCurveMeshBuilder.EmphasisType |
ThroughCurveMeshBuilder.EmphasisType.CROSS
Emphasis on cross strings.
|
static ThroughCurveMeshBuilder.EmphasisType |
ThroughCurveMeshBuilder.EmphasisType.PRIMARY
Emphasis on primary strings.
|
Modifier and Type | Method and Description |
---|---|
ThroughCurveMeshBuilder.EmphasisType |
ThroughCurveMeshBuilder.emphasis()
Returns the emphasis options.
|
static ThroughCurveMeshBuilder.EmphasisType |
ThroughCurveMeshBuilder.EmphasisType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ThroughCurveMeshBuilder.EmphasisType |
ThroughCurveMeshBuilder.EmphasisType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ThroughCurveMeshBuilder.EmphasisType[] |
ThroughCurveMeshBuilder.EmphasisType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ThroughCurveMeshBuilder.setEmphasis(ThroughCurveMeshBuilder.EmphasisType emphasis)
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.