Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ThroughCurveMeshBuilder.BodyPreferenceTypes |
ThroughCurveMeshBuilder.BodyPreferenceTypes.SHEET
Sheet
|
static ThroughCurveMeshBuilder.BodyPreferenceTypes |
ThroughCurveMeshBuilder.BodyPreferenceTypes.SOLID
Solid
|
Modifier and Type | Method and Description |
---|---|
ThroughCurveMeshBuilder.BodyPreferenceTypes |
ThroughCurveMeshBuilder.bodyPreference()
Returns the body type options
License requirements: None. |
static ThroughCurveMeshBuilder.BodyPreferenceTypes |
ThroughCurveMeshBuilder.BodyPreferenceTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ThroughCurveMeshBuilder.BodyPreferenceTypes |
ThroughCurveMeshBuilder.BodyPreferenceTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ThroughCurveMeshBuilder.BodyPreferenceTypes[] |
ThroughCurveMeshBuilder.BodyPreferenceTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ThroughCurveMeshBuilder.setBodyPreference(ThroughCurveMeshBuilder.BodyPreferenceTypes bodyPreference)
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.