Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SymmetricBuilder.PlaneOptions |
SymmetricBuilder.PlaneOptions.EXISTING
existing plane
|
static SymmetricBuilder.PlaneOptions |
SymmetricBuilder.PlaneOptions.NEW
new plane
|
Modifier and Type | Method and Description |
---|---|
SymmetricBuilder.PlaneOptions |
SymmetricBuilder.symmetryPlaneOption()
Returns the symmetry plane option.
|
static SymmetricBuilder.PlaneOptions |
SymmetricBuilder.PlaneOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SymmetricBuilder.PlaneOptions |
SymmetricBuilder.PlaneOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SymmetricBuilder.PlaneOptions[] |
SymmetricBuilder.PlaneOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SymmetricBuilder.setSymmetryPlaneOption(SymmetricBuilder.PlaneOptions symmetryPlaneOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.