Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StyledCornerBuilder.CurveControlTypes |
StyledCornerBuilder.CurveControlTypes.BOTTOM_BRIDGE_CURVE
Use bottom curve
|
static StyledCornerBuilder.CurveControlTypes |
StyledCornerBuilder.CurveControlTypes.ISO_CURVE_U
Use iso u curve
|
static StyledCornerBuilder.CurveControlTypes |
StyledCornerBuilder.CurveControlTypes.ISO_CURVE_V
Use iso v curve
|
static StyledCornerBuilder.CurveControlTypes |
StyledCornerBuilder.CurveControlTypes.TOP_BASE_CURVE
Use top curve
|
Modifier and Type | Method and Description |
---|---|
StyledCornerBuilder.CurveControlTypes |
StyledCornerBuilder.curveControl()
Returns the curve control
License requirements: None. |
static StyledCornerBuilder.CurveControlTypes |
StyledCornerBuilder.CurveControlTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StyledCornerBuilder.CurveControlTypes |
StyledCornerBuilder.CurveControlTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StyledCornerBuilder.CurveControlTypes[] |
StyledCornerBuilder.CurveControlTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StyledCornerBuilder.setCurveControl(StyledCornerBuilder.CurveControlTypes curveControl)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
void |
StyledCornerBuilder.updateOnPathDimPath(StyledCornerBuilder.CurveControlTypes curveControlOption,
int startEndIndex)
Gets the path in current position and sets it in builder.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.