Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioXformBuilderEx.ScalingCenterType |
StudioXformBuilderEx.ScalingCenterType.SCALEABOUTOBJECTCENTER
Scale center at the object center
|
static StudioXformBuilderEx.ScalingCenterType |
StudioXformBuilderEx.ScalingCenterType.SCALEABOUTPOINT
Scale center at a point
|
static StudioXformBuilderEx.ScalingCenterType |
StudioXformBuilderEx.ScalingCenterType.SCALEABOUTSELECTED
Scale center at the selected object
|
Modifier and Type | Method and Description |
---|---|
StudioXformBuilderEx.ScalingCenterType |
StudioXformBuilderEx.scalingCenter()
Returns the scaling center
License requirements: None. |
static StudioXformBuilderEx.ScalingCenterType |
StudioXformBuilderEx.ScalingCenterType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioXformBuilderEx.ScalingCenterType |
StudioXformBuilderEx.ScalingCenterType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioXformBuilderEx.ScalingCenterType[] |
StudioXformBuilderEx.ScalingCenterType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioXformBuilderEx.setScalingCenter(StudioXformBuilderEx.ScalingCenterType scalingCenter)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.