Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioXformBuilderEx.ProportionalPoleControlType |
StudioXformBuilderEx.ProportionalPoleControlType.ALL
All poles are moved
|
static StudioXformBuilderEx.ProportionalPoleControlType |
StudioXformBuilderEx.ProportionalPoleControlType.BY_UV
Poles on U or V are moved
|
static StudioXformBuilderEx.ProportionalPoleControlType |
StudioXformBuilderEx.ProportionalPoleControlType.SELECTED
Only selected poles are moved
|
Modifier and Type | Method and Description |
---|---|
StudioXformBuilderEx.ProportionalPoleControlType |
StudioXformBuilderEx.proportionalPoleControlOption()
Returns the proportional pole control type
License requirements: None. |
static StudioXformBuilderEx.ProportionalPoleControlType |
StudioXformBuilderEx.ProportionalPoleControlType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioXformBuilderEx.ProportionalPoleControlType |
StudioXformBuilderEx.ProportionalPoleControlType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioXformBuilderEx.ProportionalPoleControlType[] |
StudioXformBuilderEx.ProportionalPoleControlType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioXformBuilderEx.setProportionalPoleControlOption(StudioXformBuilderEx.ProportionalPoleControlType poleControlOption)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.