Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioXformBuilder.ScalingCenterType |
StudioXformBuilder.ScalingCenterType.ABOUT_OBJECT_CENTER
Scale center at the object center
|
static StudioXformBuilder.ScalingCenterType |
StudioXformBuilder.ScalingCenterType.ABOUT_POINT
Scale center at a point
|
static StudioXformBuilder.ScalingCenterType |
StudioXformBuilder.ScalingCenterType.ABOUT_SELECTED_OBJECT
Scale center at the selected object
|
Modifier and Type | Method and Description |
---|---|
StudioXformBuilder.ScalingCenterType |
StudioXformBuilder.scalingCenter()
Deprecated.
Deprecated in NX8.5.0. Use
StudioXformBuilderEx instead.
|
static StudioXformBuilder.ScalingCenterType |
StudioXformBuilder.ScalingCenterType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioXformBuilder.ScalingCenterType |
StudioXformBuilder.ScalingCenterType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioXformBuilder.ScalingCenterType[] |
StudioXformBuilder.ScalingCenterType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioXformBuilder.setScalingCenter(StudioXformBuilder.ScalingCenterType scaleCenter)
Deprecated.
Deprecated in NX8.5.0. Use
StudioXformBuilderEx instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.