Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioXformBuilder.RotatingPivotType |
StudioXformBuilder.RotatingPivotType.ABOUT_OBJECT_CENTER
Rotate pivot at the object center
|
static StudioXformBuilder.RotatingPivotType |
StudioXformBuilder.RotatingPivotType.ABOUT_POINT
Rotate pivot at a point
|
static StudioXformBuilder.RotatingPivotType |
StudioXformBuilder.RotatingPivotType.ABOUT_SELECTED_OBJECT
Rotate pivot at the selected object
|
Modifier and Type | Method and Description |
---|---|
StudioXformBuilder.RotatingPivotType |
StudioXformBuilder.rotatingPivot()
Deprecated.
Deprecated in NX8.5.0. Use
StudioXformBuilderEx instead.
|
static StudioXformBuilder.RotatingPivotType |
StudioXformBuilder.RotatingPivotType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioXformBuilder.RotatingPivotType |
StudioXformBuilder.RotatingPivotType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioXformBuilder.RotatingPivotType[] |
StudioXformBuilder.RotatingPivotType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioXformBuilder.setRotatingPivot(StudioXformBuilder.RotatingPivotType rotatePivot)
Deprecated.
Deprecated in NX8.5.0. Use
StudioXformBuilderEx instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.