Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioXformBuilder.PlanarizeDirectionType |
StudioXformBuilder.PlanarizeDirectionType.U
U direction when planarize
|
static StudioXformBuilder.PlanarizeDirectionType |
StudioXformBuilder.PlanarizeDirectionType.V
V direction when planarize
|
Modifier and Type | Method and Description |
---|---|
StudioXformBuilder.PlanarizeDirectionType |
StudioXformBuilder.planarizeDirection()
Deprecated.
Deprecated in NX8.5.0. Use
StudioXformBuilderEx instead.
|
static StudioXformBuilder.PlanarizeDirectionType |
StudioXformBuilder.PlanarizeDirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioXformBuilder.PlanarizeDirectionType |
StudioXformBuilder.PlanarizeDirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioXformBuilder.PlanarizeDirectionType[] |
StudioXformBuilder.PlanarizeDirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioXformBuilder.setPlanarizeDirection(StudioXformBuilder.PlanarizeDirectionType planarizeDirection)
Deprecated.
Deprecated in NX8.5.0. Use
StudioXformBuilderEx instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.