Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioSplineBuilderEx.DrawingPlaneOptions |
StudioSplineBuilderEx.DrawingPlaneOptions.GENERAL
General plane
|
static StudioSplineBuilderEx.DrawingPlaneOptions |
StudioSplineBuilderEx.DrawingPlaneOptions.VIEW
View plane
|
static StudioSplineBuilderEx.DrawingPlaneOptions |
StudioSplineBuilderEx.DrawingPlaneOptions.XY
XY plane
|
static StudioSplineBuilderEx.DrawingPlaneOptions |
StudioSplineBuilderEx.DrawingPlaneOptions.XZ
XZ plane
|
static StudioSplineBuilderEx.DrawingPlaneOptions |
StudioSplineBuilderEx.DrawingPlaneOptions.YZ
YZ plane
|
Modifier and Type | Method and Description |
---|---|
StudioSplineBuilderEx.DrawingPlaneOptions |
StudioSplineBuilderEx.drawingPlaneOption()
Returns a drawing plane option
License requirements: None. |
static StudioSplineBuilderEx.DrawingPlaneOptions |
StudioSplineBuilderEx.DrawingPlaneOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioSplineBuilderEx.DrawingPlaneOptions |
StudioSplineBuilderEx.DrawingPlaneOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioSplineBuilderEx.DrawingPlaneOptions[] |
StudioSplineBuilderEx.DrawingPlaneOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioSplineBuilderEx.setDrawingPlaneOption(StudioSplineBuilderEx.DrawingPlaneOptions planeOption)
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.