Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioSplineBuilder.MatchKnotsType |
StudioSplineBuilder.MatchKnotsType.CUBIC
Match knots for cubic non-periodic spline
|
static StudioSplineBuilder.MatchKnotsType |
StudioSplineBuilder.MatchKnotsType.GENERAL
Match knots for general spline
|
static StudioSplineBuilder.MatchKnotsType |
StudioSplineBuilder.MatchKnotsType.NONE
No knot matching
|
Modifier and Type | Method and Description |
---|---|
StudioSplineBuilder.MatchKnotsType |
StudioSplineBuilder.matchKnots()
Deprecated.
Deprecated in NX8.0.0. Use
StudioSplineBuilderEx instead.
|
static StudioSplineBuilder.MatchKnotsType |
StudioSplineBuilder.MatchKnotsType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioSplineBuilder.MatchKnotsType |
StudioSplineBuilder.MatchKnotsType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioSplineBuilder.MatchKnotsType[] |
StudioSplineBuilder.MatchKnotsType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioSplineBuilder.setMatchKnots(StudioSplineBuilder.MatchKnotsType matchKnots)
Deprecated.
Deprecated in NX8.0.0. Use
StudioSplineBuilderEx instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.