Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioSplineBuilder.CurveOption |
StudioSplineBuilder.CurveOption.BLANK
Blank input curve
|
static StudioSplineBuilder.CurveOption |
StudioSplineBuilder.CurveOption.DELETE
Delete input curve
|
static StudioSplineBuilder.CurveOption |
StudioSplineBuilder.CurveOption.RETAIN
Retain input curve
|
Modifier and Type | Method and Description |
---|---|
StudioSplineBuilder.CurveOption |
StudioSplineBuilder.inputCurveOption()
Deprecated.
Deprecated in NX8.0.0. Use
StudioSplineBuilderEx instead.
|
static StudioSplineBuilder.CurveOption |
StudioSplineBuilder.CurveOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioSplineBuilder.CurveOption |
StudioSplineBuilder.CurveOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioSplineBuilder.CurveOption[] |
StudioSplineBuilder.CurveOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioSplineBuilder.setInputCurveOption(StudioSplineBuilder.CurveOption option)
Deprecated.
Deprecated in NX8.0.0. Use
StudioSplineBuilderEx instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.