Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StepBuilder.ReferenceBoundaryTypes |
StepBuilder.ReferenceBoundaryTypes.CURVE
Select section curves as reference boundary object
|
static StepBuilder.ReferenceBoundaryTypes |
StepBuilder.ReferenceBoundaryTypes.DATUM_PLANE
Select datum plane as reference boundary object
|
static StepBuilder.ReferenceBoundaryTypes |
StepBuilder.ReferenceBoundaryTypes.EDGE
Select edges as reference boundary object
|
static StepBuilder.ReferenceBoundaryTypes |
StepBuilder.ReferenceBoundaryTypes.FACE
Select faces as reference boundary object
|
Modifier and Type | Method and Description |
---|---|
StepBuilder.ReferenceBoundaryTypes |
StepBuilder.refObjectType1()
Returns the reference object type 1
License requirements: None. |
StepBuilder.ReferenceBoundaryTypes |
StepBuilder.refObjectType2()
Returns the reference object type 2
License requirements: None. |
static StepBuilder.ReferenceBoundaryTypes |
StepBuilder.ReferenceBoundaryTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StepBuilder.ReferenceBoundaryTypes |
StepBuilder.ReferenceBoundaryTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StepBuilder.ReferenceBoundaryTypes[] |
StepBuilder.ReferenceBoundaryTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StepBuilder.setRefObjectType1(StepBuilder.ReferenceBoundaryTypes refObjectType1)
License requirements: nx_aero_design (" NX Aero Design") . |
void |
StepBuilder.setRefObjectType2(StepBuilder.ReferenceBoundaryTypes refObjectType2)
License requirements: nx_aero_design (" NX Aero Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.