Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SilhouetteFlangeBuilder.ReferenceDirectionOptions |
SilhouetteFlangeBuilder.ReferenceDirectionOptions.FACE_NORMAL
Create flange along face normal
|
static SilhouetteFlangeBuilder.ReferenceDirectionOptions |
SilhouetteFlangeBuilder.ReferenceDirectionOptions.NORMAL_DRAFT
Create flange along silhouette curve and face normal
|
static SilhouetteFlangeBuilder.ReferenceDirectionOptions |
SilhouetteFlangeBuilder.ReferenceDirectionOptions.VECTOR
Create flange along reference vector
|
static SilhouetteFlangeBuilder.ReferenceDirectionOptions |
SilhouetteFlangeBuilder.ReferenceDirectionOptions.VECTOR_DRAFT
Create flange along silhouette curve and reference vector
|
Modifier and Type | Method and Description |
---|---|
SilhouetteFlangeBuilder.ReferenceDirectionOptions |
SilhouetteFlangeBuilder.referenceDirectionOption()
Returns the reference direction option
License requirements: None. |
static SilhouetteFlangeBuilder.ReferenceDirectionOptions |
SilhouetteFlangeBuilder.ReferenceDirectionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SilhouetteFlangeBuilder.ReferenceDirectionOptions |
SilhouetteFlangeBuilder.ReferenceDirectionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SilhouetteFlangeBuilder.ReferenceDirectionOptions[] |
SilhouetteFlangeBuilder.ReferenceDirectionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SilhouetteFlangeBuilder.setReferenceDirectionOption(SilhouetteFlangeBuilder.ReferenceDirectionOptions referenceDirectionOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.