Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SilhouetteFlangeBuilder.OutputSurfaceOptions |
SilhouetteFlangeBuilder.OutputSurfaceOptions.BLEND_FLANGE
Output blend and flange surfaces
|
static SilhouetteFlangeBuilder.OutputSurfaceOptions |
SilhouetteFlangeBuilder.OutputSurfaceOptions.FLANGE_ONLY
Output flange surface
|
static SilhouetteFlangeBuilder.OutputSurfaceOptions |
SilhouetteFlangeBuilder.OutputSurfaceOptions.PIPE_ONLY
Output pipe
|
Modifier and Type | Method and Description |
---|---|
SilhouetteFlangeBuilder.OutputSurfaceOptions |
SilhouetteFlangeBuilder.outputSurfaceOption()
Returns the output surface option
License requirements: None. |
static SilhouetteFlangeBuilder.OutputSurfaceOptions |
SilhouetteFlangeBuilder.OutputSurfaceOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SilhouetteFlangeBuilder.OutputSurfaceOptions |
SilhouetteFlangeBuilder.OutputSurfaceOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SilhouetteFlangeBuilder.OutputSurfaceOptions[] |
SilhouetteFlangeBuilder.OutputSurfaceOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SilhouetteFlangeBuilder.setOutputSurfaceOption(SilhouetteFlangeBuilder.OutputSurfaceOptions outputSurfaceOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.