Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ShelfBuilder.Types |
ShelfBuilder.Types.END |
static ShelfBuilder.Types |
ShelfBuilder.Types.MIDDLE |
Modifier and Type | Method and Description |
---|---|
ShelfBuilder.Types |
ShelfBuilder.shelfType()
Returns the type
License requirements: None. |
static ShelfBuilder.Types |
ShelfBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShelfBuilder.Types |
ShelfBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShelfBuilder.Types[] |
ShelfBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ShelfBuilder.setShelfType(ShelfBuilder.Types type)
License requirements: nx_aero_design (" NX Aero Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.