Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SectionSurfaceBuilderEx.Spine |
SectionSurfaceBuilderEx.Spine.BY_CURVE
spine by curve
|
static SectionSurfaceBuilderEx.Spine |
SectionSurfaceBuilderEx.Spine.BY_VECTOR
spine by vector
|
Modifier and Type | Method and Description |
---|---|
SectionSurfaceBuilderEx.Spine |
SectionSurfaceBuilderEx.spineType()
Returns the spine.
|
static SectionSurfaceBuilderEx.Spine |
SectionSurfaceBuilderEx.Spine.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionSurfaceBuilderEx.Spine |
SectionSurfaceBuilderEx.Spine.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionSurfaceBuilderEx.Spine[] |
SectionSurfaceBuilderEx.Spine.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionSurfaceBuilderEx.setSpineType(SectionSurfaceBuilderEx.Spine spineType)
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_2 ("advanced freeform modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.