Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SectionSurfaceBuilderEx.ConicType |
SectionSurfaceBuilderEx.ConicType.FIVE_POINT
Five Point mode
|
static SectionSurfaceBuilderEx.ConicType |
SectionSurfaceBuilderEx.ConicType.FOUR_POINT_SLOPE
Four Point Slope mode
|
static SectionSurfaceBuilderEx.ConicType |
SectionSurfaceBuilderEx.ConicType.HILITE
Hilite mode
|
static SectionSurfaceBuilderEx.ConicType |
SectionSurfaceBuilderEx.ConicType.RHO
Rho mode
|
static SectionSurfaceBuilderEx.ConicType |
SectionSurfaceBuilderEx.ConicType.SHOULDER
Shoulder mode
|
Modifier and Type | Method and Description |
---|---|
SectionSurfaceBuilderEx.ConicType |
SectionSurfaceBuilderEx.conicTypeMode()
Returns the conic type mode.
|
static SectionSurfaceBuilderEx.ConicType |
SectionSurfaceBuilderEx.ConicType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionSurfaceBuilderEx.ConicType |
SectionSurfaceBuilderEx.ConicType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionSurfaceBuilderEx.ConicType[] |
SectionSurfaceBuilderEx.ConicType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionSurfaceBuilderEx.setConicTypeMode(SectionSurfaceBuilderEx.ConicType conicTypeMode)
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_2 ("advanced freeform modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.