Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SectionSurfaceBuilderEx.CircularType |
SectionSurfaceBuilderEx.CircularType.CENTER_RADIUS
Center Radius mode
|
static SectionSurfaceBuilderEx.CircularType |
SectionSurfaceBuilderEx.CircularType.RADIUS_ANGLE_ARC
Radius Angle Arc mode
|
static SectionSurfaceBuilderEx.CircularType |
SectionSurfaceBuilderEx.CircularType.TANGENT_RADIUS
Tangent Radius mode
|
static SectionSurfaceBuilderEx.CircularType |
SectionSurfaceBuilderEx.CircularType.THREE_POINT
Three Point mode
|
static SectionSurfaceBuilderEx.CircularType |
SectionSurfaceBuilderEx.CircularType.TWO_POINT_RADIUS
Two Point Radius mode
|
static SectionSurfaceBuilderEx.CircularType |
SectionSurfaceBuilderEx.CircularType.TWO_POINT_SLOPE
Two Point Slope mode
|
Modifier and Type | Method and Description |
---|---|
SectionSurfaceBuilderEx.CircularType |
SectionSurfaceBuilderEx.circularTypeMode()
Returns the circular type mode.
|
static SectionSurfaceBuilderEx.CircularType |
SectionSurfaceBuilderEx.CircularType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionSurfaceBuilderEx.CircularType |
SectionSurfaceBuilderEx.CircularType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionSurfaceBuilderEx.CircularType[] |
SectionSurfaceBuilderEx.CircularType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionSurfaceBuilderEx.setCircularTypeMode(SectionSurfaceBuilderEx.CircularType circularTypeMode)
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_2 ("advanced freeform modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.