Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SectionSurfaceBuilder.FlowDirectionEnum |
SectionSurfaceBuilder.FlowDirectionEnum.ISO_LINE_U
flow direction follows iso u of the start surface
|
static SectionSurfaceBuilder.FlowDirectionEnum |
SectionSurfaceBuilder.FlowDirectionEnum.ISO_LINE_V
flow direction follows iso v of the start surface
|
static SectionSurfaceBuilder.FlowDirectionEnum |
SectionSurfaceBuilder.FlowDirectionEnum.NOT_SPECIFIED
flow direction not specified
|
static SectionSurfaceBuilder.FlowDirectionEnum |
SectionSurfaceBuilder.FlowDirectionEnum.PERPENDICULAR
flow direction perpendicular to the guide
|
Modifier and Type | Method and Description |
---|---|
SectionSurfaceBuilder.FlowDirectionEnum |
SectionSurfaceBuilder.endFlowDirection()
Deprecated.
Deprecated in NX9.0.0. Use
SectionSurfaceBuilderEx instead.
|
SectionSurfaceBuilder.FlowDirectionEnum |
SectionSurfaceBuilder.startFlowDirection()
Deprecated.
Deprecated in NX9.0.0. Use
SectionSurfaceBuilderEx instead.
|
static SectionSurfaceBuilder.FlowDirectionEnum |
SectionSurfaceBuilder.FlowDirectionEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionSurfaceBuilder.FlowDirectionEnum |
SectionSurfaceBuilder.FlowDirectionEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionSurfaceBuilder.FlowDirectionEnum[] |
SectionSurfaceBuilder.FlowDirectionEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionSurfaceBuilder.setEndFlowDirection(SectionSurfaceBuilder.FlowDirectionEnum endFlowDirection)
Deprecated.
Deprecated in NX9.0.0. Use
SectionSurfaceBuilderEx instead.
|
void |
SectionSurfaceBuilder.setStartFlowDirection(SectionSurfaceBuilder.FlowDirectionEnum startFlowDirection)
Deprecated.
Deprecated in NX9.0.0. Use
SectionSurfaceBuilderEx instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.