Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SectionInertiaAnalysisBuilder.Types |
SectionInertiaAnalysisBuilder.Types.EXISTING_SECTION
Existing Section Type
|
static SectionInertiaAnalysisBuilder.Types |
SectionInertiaAnalysisBuilder.Types.PARALLEL_SECTIONS
Parallel Sections Type
|
static SectionInertiaAnalysisBuilder.Types |
SectionInertiaAnalysisBuilder.Types.SECTIONS_ALONG_CURVE
Sections Along Path Type
|
Modifier and Type | Method and Description |
---|---|
SectionInertiaAnalysisBuilder.Types |
SectionInertiaAnalysisBuilder.type()
Returns the analysis
License requirements: None. |
static SectionInertiaAnalysisBuilder.Types |
SectionInertiaAnalysisBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionInertiaAnalysisBuilder.Types |
SectionInertiaAnalysisBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionInertiaAnalysisBuilder.Types[] |
SectionInertiaAnalysisBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionInertiaAnalysisBuilder.setType(SectionInertiaAnalysisBuilder.Types type)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.