Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static RibBuilder.RibThicknessOffsetOptions |
RibBuilder.RibThicknessOffsetOptions.ASYMMETRIC
Asymmetric Offset
|
static RibBuilder.RibThicknessOffsetOptions |
RibBuilder.RibThicknessOffsetOptions.SYMMETRIC
Symmetric Offset
|
Modifier and Type | Method and Description |
---|---|
RibBuilder.RibThicknessOffsetOptions |
RibBuilder.ribThicknessOffsetOption()
Returns the rib walls offset type
License requirements: None. |
static RibBuilder.RibThicknessOffsetOptions |
RibBuilder.RibThicknessOffsetOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RibBuilder.RibThicknessOffsetOptions |
RibBuilder.RibThicknessOffsetOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RibBuilder.RibThicknessOffsetOptions[] |
RibBuilder.RibThicknessOffsetOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RibBuilder.setRibThicknessOffsetOption(RibBuilder.RibThicknessOffsetOptions ribThicknessOffsetOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.