Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static RibBuilder.RibCapGeometryOptions |
RibBuilder.RibCapGeometryOptions.FROM_SECTION
Cap from section
|
static RibBuilder.RibCapGeometryOptions |
RibBuilder.RibCapGeometryOptions.FROM_SELECTED
Cap from selected
|
Modifier and Type | Method and Description |
---|---|
RibBuilder.RibCapGeometryOptions |
RibBuilder.ribCapGeometryOption()
Returns the rib cap geometry
License requirements: None. |
static RibBuilder.RibCapGeometryOptions |
RibBuilder.RibCapGeometryOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RibBuilder.RibCapGeometryOptions |
RibBuilder.RibCapGeometryOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RibBuilder.RibCapGeometryOptions[] |
RibBuilder.RibCapGeometryOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RibBuilder.setRibCapGeometryOption(RibBuilder.RibCapGeometryOptions ribCapGeometryOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.