Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ResizeChamferBuilder.SectionType |
ResizeChamferBuilder.SectionType.ASYMMETRIC_OFFSET |
static ResizeChamferBuilder.SectionType |
ResizeChamferBuilder.SectionType.OFFSETAND_ANGLE |
static ResizeChamferBuilder.SectionType |
ResizeChamferBuilder.SectionType.SYMMETRIC_OFFSET |
Modifier and Type | Method and Description |
---|---|
ResizeChamferBuilder.SectionType |
ResizeChamferBuilder.chamferType()
Returns the chamfer type
License requirements: None. |
static ResizeChamferBuilder.SectionType |
ResizeChamferBuilder.SectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ResizeChamferBuilder.SectionType |
ResizeChamferBuilder.SectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ResizeChamferBuilder.SectionType[] |
ResizeChamferBuilder.SectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ResizeChamferBuilder.setChamferType(ResizeChamferBuilder.SectionType chamferType)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.