Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ReplaceFaceBuilder.ReplaceTypes |
ReplaceFaceBuilder.ReplaceTypes.REPLACE
This stands for replace type - to replace the surface of the target face with the tool face
|
static ReplaceFaceBuilder.ReplaceTypes |
ReplaceFaceBuilder.ReplaceTypes.SIMPLIFY
This stands for simplify type - to simplify the geometry representation of a surface of a face
|
Modifier and Type | Method and Description |
---|---|
ReplaceFaceBuilder.ReplaceTypes |
ReplaceFaceBuilder.type()
Returns the replace face type, don't use it until further notification
License requirements: None. |
static ReplaceFaceBuilder.ReplaceTypes |
ReplaceFaceBuilder.ReplaceTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ReplaceFaceBuilder.ReplaceTypes |
ReplaceFaceBuilder.ReplaceTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ReplaceFaceBuilder.ReplaceTypes[] |
ReplaceFaceBuilder.ReplaceTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ReplaceFaceBuilder.setType(ReplaceFaceBuilder.ReplaceTypes replaceType)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.