Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static RadialDimensionBuilder.ValueOption |
RadialDimensionBuilder.ValueOption.DIAMETER |
static RadialDimensionBuilder.ValueOption |
RadialDimensionBuilder.ValueOption.RADIUS |
Modifier and Type | Method and Description |
---|---|
RadialDimensionBuilder.ValueOption |
RadialDimensionBuilder.radiusDiameterOption()
Returns the radius diameter option
License requirements: None. |
static RadialDimensionBuilder.ValueOption |
RadialDimensionBuilder.ValueOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RadialDimensionBuilder.ValueOption |
RadialDimensionBuilder.ValueOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RadialDimensionBuilder.ValueOption[] |
RadialDimensionBuilder.ValueOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RadialDimensionBuilder.setRadiusDiameterOption(RadialDimensionBuilder.ValueOption radiusDiameterOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.